Part Number: TUSB8041
Hi,
When I connected the USB device to the hub using TUSB8041, i got a report that I could not recognize.
Below is the state of USB.
1. Connect USB3.0 hub using TUSB8041 to PC,
Of the "Device Descriptor" of the USB3.0 hub,
I can not recognize "BOS Descriptor".
2. If you connect the USB hub in two stages, the hub of the far side from the personal computer
I can see "BOS Description", but I can not recognize the device of the nearby hub.
3. When PC-HUB 1 is connected
BOS Descriptor of HUB 1: I can not recognize (invisible).
4. When PC-HUB1-HUB2 is connected
BOS Descripter of "HUB 1": I can not recognize (invisible)
BOS Descriptor of "HUB 2": Recognizable (visible)
Is not that the problem of TUSB8041, it is a problem of USB Driver?
Please tell me the solution.
Best regard
cafain