Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB940-Q1: FPD Link III Repeater/Buffer

We have a recorder module with a a DS90UB940 and are developing a camera module with a DS90UB921 (50ohm coax). Sometimes we may need to use an extender module between the recorder and camera module. This will exceed the maximum connector count. My current thinking is that we may need a buffer or repeater in the extender module to compensate. We'll want to support both lanes in the future so I was thinking to use a DS90UH947 and DS90UH948 as a repeater pair but wondered if there maybe a simpler solution?