Part Number: TPS65981
Other Parts Discussed in Thread: TPS65982
My customer needs following clarifications on TPS65981.
- Other than Thunderbolt what all are the differences between TPS65981 and TPS65982? Also we have seen like Realtime VBUS monitoring is not present in TPS65981 compared to TPS65982. What is the advantage/necessity of Realtime VBUS?
- As we understand TPS65981 firmware has two potions - boot code which is non flashable and application code which is flashable.
- Application code is to be flashed in external flash memory, is it a must or Is there a varient with internal flash ?
- For flashing application code which all mechanisms can we use?
- Using I2C can we flash
Is there any Linux based Solution available for this TPS6598x family?