Part Number: TUSB320
Other Parts Discussed in Thread: TUSB322, TUSB321, TUSB542
Dear Team,
We are designing a portable gaming console and we want to use the USB 3.0 in a type C connector.
As per the USB controller, we have seen that your TUSB320 IC may fit on our product. Our requirements are listed below:
- USB 3.0.
- Type C connector.
- Insertion and orientation detection.
- Dual Role Port (DRP).
- VBUS detection.
- Mode detection.
- Small size.
The only issue we have found with the IC is that, according to the datasheet, it seems that the TUSB320 is USB2.0 oriented, so we are wondering if is possible use it with USB3.0 in DRP mode.
I hope you can reply us and give us some other recommendation in the case the TUSB320 won’t fit our requirements.
In advance, thank you very much.
Regards,
Jesús