Part Number: TUSB9261
Hello,
My device is using a SATA SSD and the application processor communicates to it over SS USB through the TUSB9261. I plan to make the TUSB9261's HS interface available to an external PC so the Flash can be programmed during development, but only the SS lines will be connected to the APQ during normal operation.
My question is, will this cause some problem if only the SS lines are connected to the TUSB9261 and the HS lines are unused?
Also, does this change the way the VBUS detect pin on the TUSB9261 should be used? i.e. permanently held to 0.5V by voltage divider? Only HS USB connected should raise this pin voltage?
I couldn't find much information in the datasheet regarding this.
Thanks,
Mark