This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83849I: About the operation of LINK_INT in the MICR control register

Part Number: DP83849I


Hi,

Our customer will use DP83849I in their application.
I have a question about the operation of LINK_INT in the MICR control register.

Since the meaning of LINK_INT(bit 13) means "1" when the change of Link Status,
is it correct with the recognition that it will be "1" whether Link up or Link down?

Best Regards,
Hiroaki Masumoto