Part Number: DP83848C
Hi,
I have a customer using DP83848C in their products.
A communication abnormality occurs during operation of a system.
■Issue
The LED indicates the following state.(LED configuration is Mode 1)
・Link LED is ON(Good link)
・Speed LED is ON(100Mbps)
When reading the BMSR register, the link status bit is zero.(0 = Link not established)
In this case,it is not possible to communicate at all.
■Question
Do you know the reason why BMSR register value does not match LED indication?
Best regards,
Seishin