Part Number: TUSB7340
Hello
Regarding to the connecting USB on TUSB7340, my customer is asking question.
(Their requirement configuration)
・USB3.0 device -> USB3.0 connecter -> TUSB7340 is operated as USB2.0
All(4) DN ports : USB3.0 device -> USB3.0 connecter
2x DN ports : TUSB7340 is operated as USB2.0.
2x DN ports : TUSB7340 is operated as USB3.0.
(They refer TUSB7340 EVM schematics(below) as USB3.0 connecter )
(Question)
Can this device be supported their above configuration as specification? (USB standard or TUSB7340)
If it can be supported, how does TUSB7340 configure the register?
I know that it will be supported with following configuration.
・USB2.0 device -> USB3.0 connecter -> TUSB7340 is operated as USB2.0.
(TUSB7340 EVM schematics)
But I’m not sure whether it can be supported with their requirement configuration.
Regards,
Tao_2199