Part Number: TPS65982-EVM
Hi,
I tried using the Apple multiport AV adapter powered by an Apple 61W USB-C power adapter but I don't manage to negotiate the 20V 3A profile, I only get 5V 500 mA. I made the test without the adapter, powering directly the TPS65982-EVM by the Apple 61W USB-C power adapter and I get the 20V 3A profile. The Apple multiport AV adapter should be able to be powered by the 61W power adapter as it is used to charge the Macbook. Has anyone encountered this issue ? Did I do something wrong ?
Regards,
Mehdi