Part Number: DS125BR401A
Hi,
I am using the DS125BR401A Linear Repeater in two places. One is for a x4 PCIe. The other is only a x2 but I want to use the same part to minimize the types of parts on the BOM. To terminate the unused inputs, I was going to pull the “+” input to VDD with a 1K resistor. The “-“ input in pulled to GND with a 1K.
I didn’t see anything in the data sheet about this. Is this reasonable? If not, how should they be terminated?
Thanks,
David