This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913A-Q1: DS90UB913A-Q1 characteristics shift with temperature

Part Number: DS90UB913A-Q1


I would like to confirm the characterisitics shift with temperature. of DS90UB913A-Q1.

1. How does the current consumption change with temperature change?
2. How does the limit of line rate (pixel clock) change with temperature change?
3. Do you have the data for No.1 and No.2?
4. Do we need to have the margine of line rate for the temperature change?
Can we use 100MHz clock (1.4Gbps) for overall temperature change?

Best regards,
Atsushi Yamauchi