Part Number: SN65HVD235
SN65HVD235DR, RS at continuous use with a 51KOkm. setup to run 250k Baud rate in software. Will the component be damaged if we attempt to run it at 500K baud rate?
We currently have a customer that was running them as 500K and the following happen.
1 unit exhibit problems with message transfer communicating to an external device
1 unit CAN does not start after initially communicating to an external device
1 unit still works with no issue communicating to an external device
We are trying to see if due to the RS pin pull down with a 51KOhm will create this issue so we can instruct our customer on why these issues happen.