This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High speed board design



Hi 

I am designing a IC validation board where i need to measure the Voltage, Current, SI Parameter (Vih, Voh, Overshoot, Undershoot etc),Timing Parameter(Set up and hold time) and Clock Integrity (Frequency, jitter). 

We are having SPI,SDIO,QSPI,Ethernet interfaces.

So testing prospective which provision we need to give in board so that while testing time we should not face difficulty in measuring the signal?

I am planning to use http://www.digikey.com/product-detail/en/mill-max-manufacturing-corp/2308-2-00-44-00-00-07-0/ED1063-ND/435247  as a test point so that we can easily connect the probe to the signal. Is it ok? 

Does it create any signal issue ? What all option i can use ?

Thanks

Ashutosh