Part Number: TFP401A-EP
Other Parts Discussed in Thread: TFP401, SN75LVDS83B
Hi All,
Looking for an HDMi to LVDS interface. While browsing through the website i found TFP401 and SN75LVDS83B suitable for my design.
I have few issues in concern with design using these 2 ics. Please clarify the following points.
1. How do i connect the I2C lines from the HDMI interface.
2. Does these devices require any software to be run. Or these devices are self sufficient with the minimum hardware settings.
3. Should i route the HDMI signals directly to TFP401 or should there be any buffer in between. If so suggest the buffer that needs to be used.
4. If i need to send any configuration data to display, how that needs to be transmitted.
5. what happens if power on and power off sequence are not followed.
Requesting for quick response as i am in mid of the design and needs to deliver by 1st week of March2017.
Thanks and Regards
Chiru