Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB7320: TUSB7320 device enumeration failing with error -71

Part Number: TUSB7320
Other Parts Discussed in Thread: TUSB7340

Hi,

I have custom board with NXP processor and TUSB7320 with PCIe interface. The usb controller is detected by PCI. Also usb 3.0 hub is getting detected.

But when i plug any device to usb 3.0 ports, its enumeration fails with error -71. I am using linux kernel 3.14.52

Following is the pci config space:

01:00.0 USB controller: Texas Instruments TUSB73x0 SuperSpeed USB 3.0 xHCI Host Controller (rev 02)
00: 4c 10 41 82 46 05 10 00 02 30 03 0c 10 00 00 00
10: 04 00 10 01 00 00 00 00 04 00 11 01 00 00 00 00
20: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
30: 00 00 00 00 40 00 00 00 00 00 00 00 14 01 00 00
40: 01 48 83 fe 08 00 00 00 05 70 b7 00 00 80 60 66
50: 00 00 00 00 08 00 00 00 00 00 00 00 00 00 00 00
60: 30 20 00 00 00 00 00 00 00 00 00 00 00 00 00 00
70: 10 c0 02 00 c3 8f 00 00 10 20 10 00 12 3c 07 00
80: 40 00 12 10 00 00 00 00 00 00 00 00 00 00 00 00
90: 00 00 00 00 10 00 00 00 00 00 00 00 00 00 00 00
a0: 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
b0: 00 00 00 00 00 00 0f 00 00 00 00 00 00 00 00 00
c0: 11 00 07 00 02 00 00 00 02 10 00 00 00 00 00 00
d0: 00 00 00 00 ab 0d 00 00 1b 00 00 00 3f 00 00 00
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

Following is the error:

root~# usb 3-2: device no response, device descriptor read/64, error -71
xhci_hcd 0000:01:00.0: Setup ERROR: setup context command for slot 1.
usb 3-2: device no response, device descriptor read/64, error -71
xhci_hcd 0000:01:00.0: Setup ERROR: setup context command for slot 1.
usb 3-2: device not accepting address 8, error -71
usb 3-2: device not accepting address 9, error -71
hub 3-0:1.0: unable to enumerate USB device on port 2

Is there any register configuration required from USB controller side for it to work?