Part Number: HD3SS3220
HELLO, can anyone please confirm me what is the maximum current consumption of the part HD3SS3220 and under which conditions?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: HD3SS3220
HELLO, can anyone please confirm me what is the maximum current consumption of the part HD3SS3220 and under which conditions?
Hello,
This data is already in the datasheet, IACTIVE MAX = 0.9mA. and typically is under the maximum recommended operating conditions VCC33=4V, VDD5=6V & max TA, with the mux active, signaling 3A & VCONN active.
Regards,
Diego
thanks i just wanted to confirm the same although i saw 0.9mA value but i also saw some other cases like the below, when are these applicable ?
VCONN current limit. VCONN will be (VCONN) disconnected above this value where the current consumptions goes above 300mA
also what is the standard of differential signaling at TXP,RXP pin 6,7 and other differntial input and outputs, is it LVDS?
how is the MUX working here , i mean we have so many X,RX lines coming out of the MUX?