This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848K: CDCLVC1104 for X1 input

Guru 20090 points

Part Number: DP83848K
Other Parts Discussed in Thread: CDCLVC1104

Hello,

Are there any problem to use CDCLVC1104 for X1 input?

VDD of CDCLVC1104 is 3.3V
Clock source of CDCLVC1104 is 25MHz +/-15ppm.

CDCLVC1104 Voh is 2.2V~2.9V and Voh is 0.1V~0.8V , additive jitter is 100fs.
DP83848K XI Vih is  2V and Vil is 0.8V.

Thus I think that there is no problem.

Is my understanding correct?

Best Regards,
Ryuji