Part Number: TPS2549-Q1
Hi,
I received the following question from my customer.
Are the TPS2549Q1 and the TPS2546Q1 satisfied with all specs of the BC1.2?
On the BC1.2 , it is specified that over 6V and 5A is not allowed as USB port at all times.
Do the TPS2549Q1 and the TPS2546Q1 follow above condition?
I think that these devices doesn't have overvoltage protection, so external circuit is required for all specs of the BC 1.2.
Is it correct?
Best Regards,
Kuramochi