Part Number: SN65C3223E
I’m working with the SN65C3223E in an application where we need to connect to a device via RS232. In this application, we do not need the automatic power down feature and have configured the circuit to disable the power down and always enable the receivers. The interface circuit is configured with capacitor values referenced in the application information for 3 V to 5.5 V supplies.
At the SN65C3223E, I’m measuring the following:
- !FORCEOFF = 5.03 V
- FORCEON = 5.03 V
- !EN = 4.6 mV
- !INVALID = 3.01 V
Based on the datasheet, I believe the drivers and receivers should be enabled however, when input signals are applied, there are no outputs on either the driver or receiver.
Am I misunderstanding how the SN65C3223E should be configured? What could cause the SN65C3223E outputs to not be enabled?
Thank you!
Dave