Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8020B: TUSB8020B Bus Powered Hub Shield connection.

Part Number: TUSB8020B

In the reference design TIDA-00287 , all shields are directly connected to ground. However, in the EVM TUSB8020BPHP, the shields are tied together, and also to ground using an RC filter.

If I am making what is essentially a usb powered hub (much like the TIDA-000287), which shield grounding scheme is recommended and why?

PS. The upstream port is connected to a battery-powered body-worn computer, and the downstream device is a camera.