Part Number: SN75DPHY440SS
I'm utilizing the SN75DPHY440SS in 4 lane configuration with default configuration parameters, sourced by a CSI-2 source. Lanes 1, 2, and 3 are correctly driven and re-drive both LP and HS signals.
Lane 0 is driven by the same source but fails to pass HS data (oddly, LP data is being passed correctly).
This "shouldn't" matter, but we are NOT abiding by lane ordering (i.e. MIPI lane 4 passes through DA0P/DA0N) - per the datasheet, that's acceptable.
Source receiver and termination is identical for each lane.
Any thoughts or similar experiences?
8.2 Typical Application, CSI-2 Implementations The DPHY440 supports 4 CSI-2 DPHY lanes plus a clock. Unlike DSI, CSI-2 does not have a back channel path. Because of this, there is no requirement on lane ordering. Because there is no lane ordering requirement, there are more combinations which can be implemented. All possible combinations are supported by the DPHY440. For all CSI-2 implementations, the polarity must be maintained between the CSI-2 Source and CSI-2 Sink. The DPHY440 does not support polarity inversion