Part Number: SN65HVD1040
hi,
my customer T... need some help regarding the wake up feature.
In my current project (consisting of several battery-driven modules), I would like to enable the system or the modules via CAN bus, so I selected the TI CAN transceiver (SD65HVD1040). In this regard I have the following questions, which are unclear to me and ask you or your CAN Expert colleagues for clarification:
- According to the datasheet, a dominant bit is longer than 5 us on the CAN bus,
can a CAN subscriber from the standby mode be awakened by the fact that this dominant bit is perceived by the receiving part of the CAN transceiver, and the transceiver can wake up.
My question is: all stations which are on the CAN bus in standby mode will wake up?
- Two CAN subscribers communicate with each other, and another subscriber is in the standby mode, which happens when a dominant bit (or a sequence thereof) occurs through this communication, in total is longer than 5 μs, this means that the CAN subscriber , Which is in the standby mode, in this case will awakened also?
- Please provide a brief description of all possible scenarios
regards,
kamal