This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75LVCP600S : Precautions when using the SATA 3 repeater

Part Number: SN75LVCP600S

Are you sure that this ic can be used as a sata 3 repeater?

I believe that it is available with a SATA3.0(6.0Gb/s)  Repeater.

At this point,

1. the TX signal from the CPU enters LVCP 600 S.

2. This signal is confirmed from LVCP 600 to enter the SATA keonnekteo RX signal.

However, I do not understand why signal number 1 should be long signal twice.

  • Hi

    I am sorry I do not completely understand the question.

    The SN75LVCP600S can be used to compensate for signal losses in SATA-3 systems.

    Since the equalization is an input function, the LVCP600S will provide the most benefit if it is placed closer to the SATA Rx inputs.

    Best Regards,

    Lee