Part Number: DS90CF384A
Other Parts Discussed in Thread: DS90CR286A
I have a design that uses the DS90CF384A running with an LVDS clock frequency of 33.5MHz to drive an LCD display which requires a min tsetup=4ns and a min thold=2ns. The DS90CF384A meets this minimum timing requirement with 4.5ns and 4ns, respectively, which the datasheet specifies at 65MHz. My LCD has now gone obsolete and I am looking at a new LCD. The new LCD manufacturer which meets all of my requirements mechanically, but is falling a bit short on the timing. The new display needs a min tsetup=8ns and a minthold=8ns. I realize that the DS90CF384A specified output timing is not likely dependent upon the RxCLKOUT frequency, but is there any relief in the setup and hold if running at 33.5MHz that might allow me to meet tsetup=8ns and thold 8ns? I know it's a stretch, but I thought I would ask since I am running out of options. Other LCD's I have looked at require major mechanical changes in the chassis design.
Is there characterization data available for tsetup and thold at different frequencies for the DS90CF384A?