Part Number: SN65LVDT250
Hello,
In our application we are using a 4x4 SN65LVDT250 cross-point switch to multiplex some clock signals.
We have the following configuration:
- Inputs:
IN4=opened
IN3=ground
IN2=Coming from a 240MHz oscillator
IN1=opened
-Outputs:
OUT4<=IN3
OUT3<=IN3
OUT2<=IN2
OUT1<=IN2
When we observe OUT3 using a scope, we observe a signal of amplitude ~10mV synchronous to the 240MHz oscillator connected to IN2.
We didn't find information about the cross-talk between inputs in the SN65LVDT250 data-sheet.
QUESTION1) Is it normal to observe such a noise?
QUESTION2) Is there any application note or document with a crosstalk characterization for the device?
Thank you very much!
With my best regards,
Eduardo Mendes