Part Number: DS80PCI102
Other Parts Discussed in Thread: SN75DP139
Hi Team,
The device also provides equalization (CTLE) and de-emphasis capabilities. The question I have is related
to the EQ. We need to know, if the EQ is also available when the devices is used on a PCIe link running at Gen1 speed (2.5Gbps)?
To me, the DS doesn’t outline this explicitly. There is a footnote in the DS (below table 2) that can be read in a way, that
CTLE is not dedicated to Gen3 only and also working when the link is running Gen1. This would correspond to our experience, but it would be much appreciated if you can confirm this.
Best regards
SF