Part Number: TPS65982
Hi Team,
We are tying to flash our config tool generated binary onto external SPI Flash for the TPS65982 using the Host Interface tool GUI.
When the SPI FW Update is complete, we get an error that validation of flash has failed.
The device goes into BOOT mode upon powerup instead of APP mode like it did on a previous spin of the board.
Here are of some of the boot flags:
SPIFlashPresent-True
Region0- True
Region1-True
Region0Invalid-True
Region1Invalid-True
Region0CRCFail-False
Region1CRCFail-False
Any idea what's going on here? What does invalid region mean?
Programming via Host Interface FW Update (i2c) completes without issues, but gives us the same boot errors.
Thanks,
Nabeel