Part Number: TMDS181
Hello,
I have a couple questions I would like to verify:
- When using 4 TMDS181, is it required to use them in I2C enabled mode in order for them to be addressable on the same I2C bus? It appears that the A0/A1 strap pins are not usable to set distinct I2C addresses unless I2C enabled mode is set.
- The TX termination strap pin can auto-detect termination if chip is in strap modes, but I would also like to verify whether or not auto-detect termination available if the chip is in I2C mode? I saw some details below from the datasheet but just want to verify that it will auto-detect when it's not connected.
Thanks and best regards,
Jerry Leung