Part Number: TLK106
We are using the TLK106 on two different hardware and are now having a problem with the link detection of the PHY when forcing 100Mb/FD. When the PHY is switched to this mode most times no link is detected and sometimes the link is detected after a very long time (> 20 seconds). This problem occures with different link partners connected so we assume it is not a problem of the PHY used at the link partner. The link partner is set to auto negotiation. To switch to forced mode we use the BMCR register and set the bits 8 and 13 and clear bit 12. Is there something alse we need to do to use forced mode with TLK106 PHY?