Part Number: TUSB3410UARTPDK
Other Parts Discussed in Thread: TUSB3410
Hi
I got the TUSB3410UARTPDK kit and installed the EEPROM burner software. I was able to download a 3410_i2c communication binary file to the EEPROM. I pulled the USB plug out and put it back. In the device manager I see a device under Human Interface Device with a VID (0451) and PID (3421) . There are two questions that I would like to get clarified
1) In the EEPROM burner,upon clicking on TUSB3410 EEPROM Bruner Instance (2.00) u will see the VID and PID as 451 and 3410. Whereas when I go to device manager the VID is 0451 but PID does not match this.Why?
2) In the device manager, I do not see the TUSB3410UART EVM label at all... Why?....
Please help. Thanks.
regards
Bala