Part Number: TPS2549
Hi,
I have a few questions about the TPS2549 datasheet specs.
- Is there leakage/error associated with low levels of cable compensation? For example, if the load current were 100mA would the Ics be reasonable close to (75uA/A)(100mA) = 7.5uA?
- Pg 18 of the datasheet section 8.3.2.1 #4 says:
- "C(COMP) in parallel with R(FA) is needed to stablilize V(OUT) when C(OUT) is large. Start with C(COMP) ≥ 3 × G(CS) × C(OUT), then adjust C(COMP) to optimize the load transient of the voltage regulator output."
- What Cout is this referring to? Is it the Cout to the "right" and/or "left" of the TPS2549?
- If configured as CDP per Table 2 CTL1-3 as '111', will the status output be active when the ILIM_LO threshold is met per section 8.3.5.2?
- If configured as CDP per Table 2 CTL1-3 as '111', but auto-switches to SDP because device didn't enumerate, will the status output be active when the ILIM_LO threshold is met per section 8.3.5.2?
Thanks!