This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65986EVM: The project template or file in TPS65986EVM

Part Number: TPS65986EVM
Other Parts Discussed in Thread: HD3SS460, , DP-EXPANSION-EVM

Hi,

I could use TPS65986EVM + DP-EXPANSION-EVM(HD3SS460, Sink Board) to implement my application. But in my design board, i need use GPIO to set/reset others chip.

I want to use the firmware in TPS65986EVM and modify GPIO setting to meet my requirement. So how could I use " TPS6598x Application Customization Tool" to load the firmware within TPS65986EVM, and modify GPIO setting.

- which one template is the firmware within TPS65986EVM?

- I found the set of template in " TPS6598x Application Customization Tool" isn't  match to TPS65986EVM's circuit. Why? Ex: GPIO0 setting of EVM circuit is  "AMSEL" , But template set AMSEL is GPIO3.

Thanks.

  • Hello,

    I would recommend starting with one of the templates for the TPS65986 in the Application Customization Tool. We have many templates configured to be used with the HD3SS460. I attached a screenshot below highlighting the different templates for the TPS65986 included with the Application Customization Tool.

    Thank you,

    Eric