This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS25BR100: the condition of Equalization Level

Part Number: DS25BR100


Hi all

Would you mind if we ask DS25BR100?

There is the description "Medium (Approx. 8 dB at 1.56 GHz)" on the datasheet P2.
In case of datarate=3.0GHz, is it possible to equalize with 8dB?

Kind regards,

Hirotaka Matsumoto

  • Hi Hirotaka,

    The DS25BR100 CTLE gain is typical ~ 8 dB @ 1.56 GHz.  This is equal to 8 dB of gain for a 3.125 Gbps data stream since the nyquist frequency of the 3.125 Gbps data is 1.56 GHz.

    The CTLE works across a relatively broad range of datarates - from approximately 1 Gbps up to the maximum 3.125 Gbps.  At the lower data rates near 1 Gbps, the CTLE gain will be less than 8 dB.

    For your case with a 3.0 Gbps data rate, the CTLE will provide ~ 8 dB of gain 

    Regards,

    Lee  

  • Quote san

    Thank you for your reply!!
    We are sorry that we misunderstand the denomination between bps and Hz.
    OK, we got it.

    Kind regards,

    Hirotaka Matsumoto