Part Number: DP83848C
Dear Texas Instrument Ethernet Forum members,
This is my first post to this forum, and I am writing this for assistance regarding an issue I am facing with my DP83848VV ethernet PHY module board. Please note it is not DP83848C as I mentioned in the part number above. it is actually DP83848VVVBI as mentioned on the chip.
My ethernet PHY module board is actually waveshare based DP83848 board:
www.waveshare.com/dp83848-ethernet-board.htm
As per the connection on this blog :
I have connected this to my STM32F4-Discovery board and developed the code with the STM32CubeMX for it. But the problem is that when I ping the board from my PC with the ethernet PHY module directly connected to my PC via a direct ethernet cable , it ping well and there is no dropout of the ethernet packets.
But when I connect it to the network via a switch in between and than I ping it through my PC than there is no communication and the message is :
Reply from 192.168.18.31: Destination host unreachable.
This is a very strange problem I am facing whereas all other PC connected to network via switch are pinging well and respond in well manner.
So I would like to get some assistance in this regard , if anybody has faced this problem before than please share your experience with me and others.
regards
Piyush Pandey