Part Number: SN75DP130
Dear Sirs
Could SN75DP130 support 1920*1080@240Hz?
If not, could you suggest what device support?
BRS
Nat
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Nat,
DP130 is designed to work with DP1.2, this supports 5.4Gbps per lane, 21.6Gbps in total which is enough for 1080p@240Hz or 4k@60Hz using 24bpp.
Regards