Part Number: TFP410
Hi,
I am giving a parallel RGB Video Input of following specifications to TFP410:
Resolution : 320x426
Frame Rate: 60 fps
Clock Frequency: 9 MHz
I couldn't get the output in TMDS lines.
I am getting output for another resolution and clock frequency using the same circuit.
- So I want to know whether the chip supports this resolution and Clock frequency.
- And also whether the chip is capable to function with and without external DE (Data Enable) Signal.
- If the clock frequency is low for TMDS lines, is it possible to perform Pixel Repetition in TFP410
Thank you in Advance!