Part Number: TUSB542
Hi
I have a simple question.
About TX pin and RX pin, there are input pin and output pin. How can we connect the those pin to the host?
At the following diagram, it is shown that TX pin(TUSB542) and TX pin(HOST) is connected.
(RX pin(TSUB542) and RX pin(HOST) is connected as well)
In general, TX pin(HOST) is connected to RX pin(downstream device). And RX pin(HOST) is connected to TX pin(downstream device).
In the case of TUSB542, Is the pin name of TUSB542 just corresponded to the pin name of HOST?
I am sorry for asking such a simple question. Because I got confused.
Regards,
Koji Hamamoto