This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8041: TUSB8041RGCR

Part Number: TUSB8041

Application : Monitor for conference

0.1uF Capacitor is connected to SERIAL between Transmitter port and USB Connector of the Differential pair line.
Does not necessarily use the function of capacitor Or it is necessary to confirm that you do not use it.
The engineer removes the appropriate Capacitor, but does not seem to have any problems.
There was no other explanation for PCB Guide line in datasheet, and there was only one thing that needed to be close to USB Connector.
Please explain why there is no capacitor in Receiver Line.

The above picture is about C2, and C3 on the Application circuit.
The same capacitor for Upstream as well as for Down stream transmitter port.
.