Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9306: Power on sequence (VREF1 and VREF2)

Part Number: PCA9306

Hi

I read some E2E post as the following,

https://e2e.ti.com/support/interface/i2c/f/390/p/420667/1498896#1498896

However I do not understand which one of VREF1 and VREF2 should we startup first. 

In our customer case, 3.3V (this should be VREF2) power on first, then after 10ms the 1.8V(this should be VREF1) start up.

Because the 1.8V is provided from 3.3V rail by DCDC.

Should we start up VREF1 first anyway?

Regards,

Koji Hamamoto