Part Number: TPD3S014
Hi, I am planning to build a board wihch is powered from the usb port (of PC). To limit current drawn from the USB to 500mA and to provide ESD protection, I want to use TPD3S014.
As mentioned in the datasheet, capacitor of minimum 120uF is recommended at the OUT pin of TPD3S014 but it is for the case where power is supplied through USB port. In our case, we only draw power from the USB. What minimum value of output capacitor is recommended for this application?
Thanks and regards,
Vinay