Part Number: TCAN1042GV-Q1
Other Parts Discussed in Thread: SN74CB3Q3251, SN74CBT3251, SN74CBTLV3251, TCAN332
Any design examples/circuits for muxing CANH/CANL onto various pins? I have a need to be able to drive these connections into various pins on the same connector. It will never be switched at run-time, and this is only done at initialization to handle connection to different pinouts. I need something on the order of a 2-to-12 mux in front of the transceiver. This will also necessitate using discrete protection circuitry to protect the mux from bus faults. Any guidance greatly appreciated.