Which ESD Modle should I consider "Human Body Model" or "Charged-Device Model for SN65HVD251DR below case?
There are two models as the condition of "Electrostatic discharge", "Human Body Model" and "Charged-Device Model" on SN65HVD251DR Datasheet Page 4 6.2 "ESD Ratings".
When the connector of cable which connected to SN65HVD251DR is connected to other charged parts, which model should I consider "Human Body Model" or "Charged-Device Model"?
Appreciate,