Part Number: CLC001
Other Parts Discussed in Thread: LMH0001,
Hi,
I would like to ask you some questions about thermal resistance as below.
My customer has been simulating the behavior with thermal.
Q1) θja and θjc value of Absolute max ratings (datasheet 3 page)
Are both data (θja=125℃/W, θjc=105℃/W) actual data or simulation data?
Q2) IDD data (datasheet 3 page)
The specification of IDD is 115mA(max) @Vsdo=800mVpp, includes load current.
Do you have the IDD data without line load, just only device power consumption?
Q3) Thermal design consideration
Would you tell me any considerations to do thermal design?
If you give me anything information to design, it will be very helpful for me.
Thank you for your support.
Best Regards,