Part Number: DP83822I
Hello,
I am looking for the relationship between RX_DV and the data content on the RX_D bus in RMII mode.
The RMII spec shows this for CRS_DV (asserted as soon as carrier detect and after a while, then preamble and data but no indication for the end of packet).
For RX_DV, the DP83822 indiactes on page 29:
"In addition, RMII mode supplies an RX_DV signal that allows a simpler method of recovering receive data
without the need to separate RX_DV from the CRS_DV indication. RX_ER is also supported even though it is not
required by the RMII specification."
So the questions are:
- is RX_DV asserted synchronously with the receiving of the preamble, and includes the whole preamble
- is RX_DV de-asserted right after the last piece of data ?
I checked on the DP83848 datasheet that provides more information, but is not fullty explicit about this (and nothing says that the two chips behave the same).
Thanks
Best regards
Pascal