Part Number: LMH0303
I'm adding an HD-SDI output to a board with no SMBus controller. Apparently, from this answer, http://e2e.ti.com/support/interface/high_speed_interface/f/138/p/410558/1458741#1458741, I can leave the SCL/SDA pins open in "pin mode". But the data sheet I have has no mention of a "pin mode". Is that just not connecting those two SMBus pins?
SD/HD is pulled down; RSTI is pulled up. RREF has 750 ohms to VCC. Is that all I need to run this part in pin mode?
Many thanks, Ken