Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65986: FW update issue when using App-customization tool, ver 2.15

Part Number: TPS65986
Other Parts Discussed in Thread: TPS65982, TPS65981

Hi team,

I could not write some project, DRP_source_Full_2_15, on the latest app-custom tool. When I try to write the setting to Flash, we always see the error below. Could you tell me how to avoid the error?

Regards,

Takashi Onawa

  • Hi Onawa-san,

    It appears that the tool did not load a Firmware Base Image for that template. I have noted this bug and will fix it for the next release of the tool.

    In the meantime, you can open any other template for the TPS65981, TPS65982, or TPS65986. On the General Settings tab you will see a Firmware Base Image option, the file that should be loaded is "tps65981_2_6_v0001.12.00.bin" Select this file for the 86 template that you are currently working on. Then you can flash the firmware to your device.

    Thank you,

    Eric

  • Hi Eric-san,

    OK, Thanks.

    Regards,
    Takashi Onawa