Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75LVCP601: Is SATA polarity relevant for chip function?

Part Number: SN75LVCP601

Hi,

Does the polarity of the connected SATA signal have any influence on the proper function of the SN75LVCP601?
E.g., is it possible to connect the redriver channels with swapped SATA_N and SATA_P e.g. HostTx+ to Rx1- and then Tx1- to SATA disk's HostTx+ and vice versa as long as the device's polarity is still correct?

This would greatly simplify routing the signals in my particular application.

Regards
Andreas