Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1: OLDI Input Port Configuration

Part Number: DS90UB947-Q1

[ DS90UB947-Q1 ] OLDI Input Port Configuration

Hi,

Can you help me to clarify the valid configuration of OLDI input port?

<Q1: OLDI_IN_MODE and OLDI_IN_SWAP descriptions>:

The description of OLDI_IN_MODE and OLDI_IN_SWAP is not straightforward...
See drawing below. It's reasonable if you say... "If OLDI_DUAL is set to 0 (single),..."
Can you comment on this? 




<Q2: DUAL_SWAP Register>:

Can you elaborate a bit more about "DUAL_SWAP" register?
Is this read only indicator? What does "1" or "0" express respectively?



Thank you for your help in advance.

Thanks,
Ken