This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD1781-Q1: Why there is need of biasing resistors in SN65HVD1781-Q1

Part Number: SN65HVD1781-Q1


Hello TI Support,

We are using 2 devices with RS485 each having SN65HVD1781-Q1. We have problem communicating both devices & will appreciate your help.

1. When we try to communicate both devices through RS-485 it doesn't work. Supply voltage of both RS-485 in each device is 3.3V & we are communicating both devices through 2- wire mode that is A & B.

2. When we added 2.2K from A to 3.3V & B to GND then communication began to work. I am not sure if SN65HVD1781-Q1 is fail safe biased then why do it require any biasing resistors? Awaiting your reply.

Thanks,

jagdish

  • Jagdish,

    1. What’s termination resistor value used, 54Ohm, 120Ohm or other value?

    2. HVD1781 can work with 3.3V to 5V power supply. But please be noted that when Vcc goes down, the output voltage decrease as well. I suggest for the first step of debug the customer check the voltages on bus for the common mode and differential values. If there is anything abnormal, we can start from there.

     

    Regards,

  • Hi Hao L,

    Thanks for your response & sorry for delayed reply. I did verified that common mode voltages amounting to 35V were present because our boards were connected with USB & ethernet from other sources working on 230VAC, 50Hz.

    Making grounds common or having 100E resistor from GND of each RS-485 to third common wire resolved the issue. Actually some RS-485 literatures recommend using 100E series resistor (from GND to third wire) to limit loop current & simultaneously creating a good reference which is within common mode range of RS-485.

    Thanks,
    jagdish
  • Jagdish,

    Great to know it works for you. Yes, connecting each node to real grounds with 100Ohm resistor could limit the loop current. But please be aware that if there is noise in the ground, it could be coupled to the signal. Please let me know if you have any questions.

    Regards,
  • Hi Hao L,

    Thanks for the information, I will make sure about ground noise.