Other Parts Discussed in Thread: TSB41BA3D
We just built 10 prototype boards with one TSB41BA3A on each board. 6 of the boards seem to work fine (both of the populated ports link to a FireSpy). The other 4 boards all have a pecular waveform on the TX+ and TX- outputs of all three ports. Unconnected ports of the working boards have a pulse 666 usec. wide with a burst of 48 MHz. These occur every 42 ms. This is the normal 1394b connection tone. The other 4 boards have an approximately 2 volt pulse, 666 usec wide every 42 ms. There is no 48 MHz toning on this pulse. I have verified the power supply voltage (correct voltage no noise), power up reset timing (200 ms for oscillator to stabalize), external oscillator etc (frequency, duty factor and amplitude okay). I can't think of anything else to look at. As soon as I can get some replacement parts I will replace the PHY chips, but in the meanwhile has anyone seen this kind problem?